SSS series solid state I/O module
provide a connection between
power lines and computer interface
systems. Input modules sense the
presence of either an ac or dc
voltage, and will send a TTL signal
back to the computer. They provide
feedback to the computer, giving the
system information it can act upon.
Output modules receive TTL signals
from the computer interface, and will
switch ac or dc power lines on or off.
These modules can be used for
control systems, turning motors,
actuators, etc. on or off.
† All dollar amounts on this site are shown in US currency.