A typical Fiber Optic Thermometer

Fiber Optics Home Page 

Fiber Optic Temperature Measurement Definition
Fiber Optics: Fiber constructed of either plastic or glass which act as a transmission path along its length for many different applications including temperature.
iR2 Series
SUPERMETER Fiber Optic Infrared Temperature Measurement & Control System
iR2 Series
From 300C up to 3000C
5 Year Warranty
Ethernet & RS232/485 Available
Full Autotune PID Control
More Info »

• Non-Contact Infrared Thermal Monitoring Systems
• Ultra High Speed Infrared Pyrometer
• High Speed I/R Detectors
• Fast Response Fiber Optic Infrared Sensors
• Fiber Optic Thermometer
• Handheld Fiber Optic Meter

immersion Heater Tech Links
• Introduction To Fiber Optics
• Controlling of Metal Production>
• 
Turbine Blade Thermal Monitoring
• Control of Semiconductor Manufacturing
• Plastic Extrusion & Injection Molding Monitoring
Figure 1
Fiber Optic Probe Construction

Using Fiber Optics
for Temperature Measurement

What is fiber optics?


Fiber optics are essentially light pipes. The group of sensors known as fiber optic thermometers generally refer to those devices measuring higher temperatures wherein blackbody radiation physics are utilized. Lower temperature targets--say from -100C to 400C--can be measured by activating various sensing materials such as phosphors, semiconductors or liquid crystals with fiber optic links offering the environmental and remoteness advantages.

Advantage of Fiber Optics

Whether used for communications or infrared temperature measurement, fiber optics offer some inherent advantages for measurements in industrial and/or harsh environments:
  • Unaffected by electromagnetic interference (EMI) from large motors, transformers, welders and the like;
  • Unaffected by radio frequency interference (RFI) from wireless communications and lightning activity;
  • Can be positioned in hard-to-reach or view places;
  • Can be focused to measure small or precise locations;
  • Does not or will not carry electrical current (ideal for explosive hazard locations);
  • Fiber cables can be run in existing conduit, cable trays or be strapped onto beams, pipes or conduit (easily installed for expansions or retrofits); and,
  • Certain cables can handle ambient temperatures to over 300C--higher with air or water purging.


Fiber Optic Applications

Fiber optic thermometers have proven invaluable in measuring temperatures in basic metals and glass productions as well as in the initial hot forming processes for such materials. Boiler burner flames and tube temperatures as well as critical turbine areas are typical applications in power generation operations. Rolling lines in steel and other fabricated metal plants also pose harsh conditions which are well handled by fiber optics.

Typical applications include furnaces of all sorts, sintering operations, ovens and kilns. Automated welding, brazing and annealing equipment often generate large electrical fields which can disturb conventional sensors.

High temperature processing operations in cement, refractory and chemical industries often use fiber optic temperature sensing. At somewhat lesser temperatures, plastics processing, paper making and food processing operations are making more use of the technology. Fiber optics are also used in fusion, sputtering, and crystal growth processes in the semiconductor industry.

Beyond direct radiant energy collection or two-color methods, fiber optic glasses can be doped to serve directly as radiation emitters at hot spots so that the fiber optics serve as both the sensor and the media. Westinghouse has developed such an approach for distributed temperature monitoring in nuclear reactors. A similar approach can be used for fire detection around turbines or jet engines. Internal "hot spot" reflecting circuitry has been incorporated to determine the location of the hot area.

An activated temperature measuring system involves a sensing head containing a luminescing phosphor attached at the tip of an optical fiber (Figure 1). A pulsed light source from the instrument package excites the phosphor to luminescence and the decay rate of the luminescence is dependent on the temperature. These methods work well for non-glowing, but hot surfaces below about 400C.

 Fiber Optic Thermometers
Infrared Thermal Monitoring Systems Monitoring Systems
The DP1511, DP1521 and DP1531 non-contact infrared thermal monitoring systems represent a unique technological approach for monitoring and controlling process temperatures. These units combine fiber optics or line-of-sight optics with advanced electronic technology into a system that continuously monitors infrared radiation (a function of temperature) in real time and without physically contacting the target material. The result is a highly reliable system offering outstanding accuracy and repeatability with high response speed.

Also...The FOB100 Series comprises high-accuracy, multipurpose fiber optic thermometers with 1, 2, or 4 channels. They use an original algorithm to analyze incoming signals, measuring the temperature on each channel.


OS4000 detector High Speed Temperature Detectors
The OS4000 series high speed industrial fiber optic infrared transmitters measure temperature ranges from 200 to 1600C (392 to 2912F) using three standard optical fields of view and three standard fiber optic cable lengths. This unit offers many standard features such as adjustable Emissivity, linear analog output, high and low alarm voltage output, RS232 PC interface, built-in laser sighting, etc. Through Windows based PC interface software, the user can select response time, Peak-Hold function, high and low alarm set points, and data logging. This unit is packaged in a space saving of 2.5" OD by 6" long. The mounting bracket and two mounting nuts are included.
iR2™ Series 2 Color Ratio Fiber Optic
The OMEGA iR2™ Series is the state-of-the-art instrument for difficult and demanding high temperature (300C-3000C) applications. It is ideally suited for measurement and control applications involving metals, glass, semiconductors and more. The iR2 is extremely fast and accurate with a response time of 10 msec and accuracy of 0.2% of full scale.
Portable Fiber Optic Data Logger Thermometer Portable Fiber Optic Handheld Devices
The HHTFO-101 offers impressive versatility. Battery operated for maximum user freedom, this single-channel instrument allows you to freely move from one area to another to measure temperatures at various critical sensing points. The HHTFO-101 is a valuable monitoring tool for a wide range of applications in energy, industrial and research activities, such as hot spot monitoring inside power transformers during manufacturing and heat runs. It can also be used in various high voltage applications and MW/RF heating applications.
^top  
Automation | Accelerometers | Calibrators | Cartridge Heaters | Chart Recorders | Cryogenics | Custom Pressure Transducers | Data Loggers | Data Acquisition | Dial Thermometers | Fiber Optics | Flexible Heaters | Flowmeters | Glass Bulb Thermometers | Grippers | Heaters | Humidity Measurement | Immersion Heaters | Infrared Thermometers | Level Measurement | Load Cells | Magnetic Flow Meters | Panel Meters | Pressure Gauges | Pressure Transducers | Rotameters | RTD| Signal Conditioners | Stepper Motors | Strain Gages | Strip Heaters | Temperature Controllers | Temperature Labels | Temperature Measurement | Temperature Sensor Manufacturing | Temperature Transmitters | Thermistors | Thermocouple | Thermocouple Wire | Thermowell | Ultrasonic Flow Meters
Home Page Order by part number Free Literature About OMEGA Engineering