Back to omega.ca
Panel Meters
 
   Introduction to Signal Conditioners



Product Links
View All Signal Conditioners
Technical Links
What is a Signal Conditioner?

Signal conditioners are devices that convert one type of electronic signal into a another type of signal. Their primary use is to convert a signal that may be difficult to read by conventional instrumentation into a more easily read format In performing this conversion a number of functions may take place. Examples of signal conditioner functions include:
  • Amplification
    When signals are amplified, the overall magnitude of the signal is increased. Converting a 0-10mV signal to a 0 -10V signal is an example of amplification.

  • Electrical Isolation
    Electrical isolation breaks the galvanic path between the input and output signal. That is, there is no physical wiring between the input and output. The input is normally tranferred to the output by converting it to an optical or magnetic signal then it is reconstructed on the output. By breaking the galvanic path between input and output, unwanted signals on the input line are prevented from passing through to the output. Isolation is required when a measurement must be made on a surface with a voltage potential far above ground. Isolation is also used to prevent ground loops.

  • Linearization
    Converting a non-linear input signal to a linear output signal. This is common for thermocouple signals.

  • Cold Junction Compensation
    Used for thermocouples. The thermocouple signal is adjusted for fluctuations in room temperature.

  • Excitation
    Many sensors require some form of excitation for them to operate. Strain gages and RTDs are two common examples.
DR-IO Series
Mini Rail Mount Input &Output Modules: DR-IO Series
Ideal for connecting real world, discrete signals, to a computer interface and other electronic equipment. The compact design permits high density mounting on a standard DIN rail.
More details »


   Type of Signal Conditioners
DIN Rail Mount
DIN rail mount signal conditioners mount on a DIN rail bracket. DIN rail conditioners are very popular in industrial applications since they provide a rugged mounting format for either a few or a large number of signal conditioners.

DRG Series Din Rail Mount Signal Conditioner
Backplane Mount Conditioners
Certain signal conditioners can also be mounted on a common backplane. The backplane style provides the advantage of all output signals being accessible through a single common connnector. The backplane style signal conditioners are often used with data acquisition systems since a single cable can connect multiple conditioners to a data acquisiton device.
OM7 Series Backplane Mount Conditioners
Digital Signal Conditioners
Digital conditioners are one of the more recent developments in signal conditioners. The output of a digital signal conditioner is converted to a digital format such as RS232, RS485 or even Ethernet. Digital signals have several advantages over analog signals. They provide a high degree of immunity from electrical noise, they can also support extended transmission distances and are easily connected to a computer. With an ethernet output, the input signal can be read across an entire network or even across the internet if so configured.
D1000 Digital Signal Conditioners
Automation | Accelerometers | Calibrators | Cartridge Heaters | Chart Recorders | Cryogenics | Custom Pressure Transducers | Data Loggers | Data Acquisition | Dial Thermometers | Fiber Optics | Flexible Heaters | Flowmeters | Glass Bulb Thermometers | Grippers | Heaters | Humidity Measurement | Immersion Heaters | Infrared Thermometers | Level Measurement | Load Cells | Magnetic Flow Meters | Panel Meters | Pressure Gauges | Pressure Transducers | Rotameters | RTD| Signal Conditioners | Stepper Motors | Strain Gages | Strip Heaters | Temperature Controllers | Temperature Labels | Temperature Measurement | Temperature Sensor Manufacturing | Temperature Transmitters | Thermistors | Thermocouple | Thermocouple Wire | Thermowell | Ultrasonic Flow Meters