Navigation image map
A typical data logger

Data Logger Home Page 

Data Logger Definition
Data Logger: Device that can read various types of electrical signals and store the data in internal memory for later download to a computer.
A Sampling of Datalogger Products
• Data Logger Product Finder
• Humidity/Temperature Data Loggers
• Data Acquistion Systems and Signal Conditioners
• ON-900 Series Precision-Interchangeable Thermistor Probes
• Linear Thermistors
• Environmental Wall Mount Thermistor Sensor
• TJ Thermistor Probes
• THX-400 Series Probes
• Thermistor Elements, Probes and Assemblies
• Wire: Thermocouple, RTD, Thermistor and Heater Hook-Up
See All Data Loggers
Datalogger Tech Links
• Using Thermistors (PDF file)
• OMEGA® Interchangeable Thermistor Applications (PDF file)
• Thermistor Resistance vs. Temperature (PDF file)
• Resistance vs. Temperature for Series 700 Linear Thermistor Pairs (PDF file)
• Temperature Measurement and Control Glossary(PDF file)
• Introduction to Temperature Measurement
• Using Thermistors (PDF file)
• Frequently Asked Temperature Questions (PDF file)
• Ohm's Law, Summary
• Handheld Thermocouple and Surface Probes
• Special Purpose Thermocouple Probes
• Industrial Thermocouple
See all Technical References
Sign up for the omega.com e-mail newsletter!
Click here to Find Data Loggers!
DC Current Data Logger
OM-CP-PROCESS101A Series
DC Current Data Logger
• 10 Year Battery Life
• 4 Hz Reading Rate • Multiple Start/Stop Function
• Ultra High Speed Download
• 1 Million Reading Storage Capacity
More Info »
Data Loggers - an Overview

What is a Data Logger?

Data loggers are any devices that are used to store data. This includes many data acquisition devices such as plug-in boards or serial communication systems which use a computer as a real time data recording system. However, most instrument manufacturers consider a data logger a stand alone device that can read various types of electrical signals and store the data in internal memory for later download to a computer.
The advantage of data loggers is that they can operate independently of a computer, unlike many other types of data acquisition devices. Dataloggers are available in various shapes and sizes. The range includes simple economical single channel fixed function loggers to more powerful programmable devices capable of handling hundreds of inputs.

How to Choose a Data Logger
When choosing a data logger the following parameters should be considered.
  • Input Signal
    OMEGA offers data loggers that are compatible with most types of signals. Some data loggers are dedicated to a certain input type while others are programmable for different types of inputs. OMEGA offers data loggers for the following types of signals.
    AC Voltage/Current  Light On/OffShock/Acceleration
    Bridge/Strain/Load/Pressure   Motor On/OffSound
    Dew pointPH PressureTemperature
    Event or StateProcess Voltage/Current  Thermistor
    FrequencyRelative HumidityThermocouple
    LevelRTD 

  • Number of Inputs
    Data Loggers are available in both single and multi-channel designs. Some data loggers are capable of handling hundreds of inputs. OMEGA's OMB-LOGBOOK-300 for example is expandable to over 400 channels.

  • Sizes
    In many applications space is a limitation. In those cases the size of the data logger may be a critical selection parameter. OMEGA's OM-CP family of data loggers are extremely compact and include models for most input types.

  • Speed and Memory
    Compared to real time data acquisition systems, data loggers generally have low sample rates. This is normally because they store data in internal memory which is limited. The higher the data rates the more memory required. Therefore when specifying a data logger it is important to determine the sample rate and the sample duration which can be used to calculate the required memory. For example. If an application requires sample rates of 1 per second and the test must last one hour, the data logger must be able to store 3600 samples(1 sample/sec x 1 hour x 3600 seconds/hour).

  • Operating in Real Time
    For some applications it may be desirable to display the data being collected in real time on a computer. Certain data loggers such as OMEGA's OM-CP family support this feature.

Data Logger FAQ's (Frequently Asked Questions)

Why Choose a Data Logger Over Other Types of Data Collection Instruments?
Three types of instruments are commonly used for collecting and storing data. They are 1)Real-Time Data Acquisition Systems, 2)Chart Recorders and 3)Data Loggers

Data loggers are normally more economical than chart recorders. They offer more flexibility and are available with a greater variety of input types. Most data loggers collect data which may be directly transferred to a computer. Although this option is available with some recorders, it normally adds significant expense to the recorder price.
Data acquisition systems offer a great deal of flexibility and are certainly attractive when high sample rates are required, however, since they require connection or installation into a computer, the computer must also be present and active when collecting the data. Data loggers can collect data independently of a computer. Data is normally collected in non-volatile memory for later download to a computer. The computer does not need to be present during the data collection process. This makes them ideally suited for applications requiring portability.

Do Data Loggers Need to be Connected to a Computer?
No, some data loggers provide an option for real-time display but all OMEGA data loggers collect data independently of the computer.

What is the Maximum Sample Rate for a Data Logger?
The sample rate depends on the specific model. Although most data loggers have a maximum data rate of 1 or 2 samples per second, OMEGA offers a number of data loggers that can sample in excess of 100 samples per second.

How are the Data Loggers Powered?
Most data loggers are battery powered some also offer an option for external power.

How Long Does the Battery Powered Logger Last?
The battery life of a data logger depends on a number of parameters including the specific model and sample rate. In general the faster the sample rate the shorter the battery life. Many OMEGA data loggers feature a battery life as long as ten years.

Will the Data Logger Loose its Data if the Power or Battery Fails ?
Most OMEGA data loggers use non-volatile memory for data storage. This means that the data will not be lost if the power fails.

How Long Can the Data Logger Record Data?
The recording duration is dependent on the memory capacity of the data logger and the desired sample rate. To determine the duration divide the memory capacity(number of samples the device can record) by the sample rate. As an example assume that a given data logger can store 10,000 samples. If it is desired to record 2 samples every minute, the data logger can run for 10,000/2 or 5,000 minutes(about 3.5 days). If the sample rate was cut in half(1 sample per minute), the recording period would double to 7 days.

 Types of Data Loggers
OM-CP-Temp100 Miniature Single-Input Data Logger Miniature Single Input Data Loggers
Miniature single input data loggers are generally low cost loggers dedicated to a specific input type. These types of data loggers are often used in the transportation industry. A typical application would be to include a temperature data logger in a shipment of food products to insure that the food temperature does not exceed acceptable limits. In addition to temperature miniature data loggers are available for a large variety of input types. most input types.

OM-CP-QUADTEMP Fixed Input Data Logger Fixed Mount Multi-Channel Data Loggers
Fixed input loggers have a fixed number of input channels which are generally dedicated for a specific type of input. OMEGA offers fixed input data loggers ranging from one to 8 channels.
OM-DAQPRO-5300 Portable Handheld Datalogger Handheld Multi-Channel Data Loggers
Handheld multi-channel loggers are commonly used in applications where the data logger is to be carried from one location to another. They are also commonly used in benchtop or laboratory environments. In addition to storing data internally some models even contain on board printers which can produce an immediate hardcopy of the data.
OM-320 Modular Data Logger Modular Data Loggers
A modular data logger is configurable and expandable through the use of plug-in modules. The modules are normally field configurable and the user has the option of adding as many channels to satisfy the application requirement.
^top  
Automation | Accelerometers | Calibrators | Cartridge Heaters | Chart Recorders | Cryogenics | Custom Pressure Transducers | Data Loggers | Data Acquisition | Dial Thermometers | Fiber Optics | Flexible Heaters | Flowmeters | Glass Bulb Thermometers | Grippers | Heaters | Humidity Measurement | Immersion Heaters | Infrared Thermometers | Level Measurement | Load Cells | Magnetic Flow Meters | Panel Meters | Pressure Gauges | Pressure Transducers | Rotameters | RTD| Signal Conditioners | Stepper Motors | Strain Gages | Strip Heaters | Temperature Controllers | Temperature Labels | Temperature Measurement | Temperature Sensor Manufacturing | Temperature Transmitters | Thermistors | Thermocouple | Thermocouple Wire | Thermowell | Ultrasonic Flow Meters
Home Page Order by part number Free Literature Search About OMEGA Engineering