Navigation Image Map

Infrared Thermometer Home 

Definition Infrared Thermometer
What is: An Infrared Thermometer (ir thermometer)? An ir thermometer is a non-contact temperature measurement device. Infrared Thermometers detect the infrared energy emitted by all materials -- at temperatures above absolute zero, (0°Kelvin)-- and converts the energy factor into a temperature reading.
OS523E and OS524E Series
High-Temperature Handheld Infrared Thermometer
OS523E and OS524E Series
• Available with Ranges to 2482°C
• Built-In Laser Sighting
• Distance-measuring option
• °C/°F selectable
• RS232 output
More Info »

Infrared Thermometer Products
Buy Infrared Thermometers!
• Infrared Selection Guide (PDF File)
• Handheld Infrared Thermometers
• Infrared Thermocouples
• Fixed Mount Infrared Thermometer/
Transmitters

• Infrared Selection Guide
• Pocket/Stick-Type Infrared Thermometers
• Handheld Infrared Thermometers
• OMEGASCOPE™ Handheld Infrared Thermometers
• Fixed Mount Infrared Thermometer/Transmitters
• Infrared Blackbody Calibrators
• Benchtop Meters
See All Infrared Thermometers
Infrared Thermometer Tech Links
• Transactions: An Omega Technical reference Publication on Infrared (PDF file)
• Principles of Infrared Thermometry (PDF file)
• Article on Infrared Temperature Measurement (PDF file)
• Introduction to Infrared Pyrometers (PDF file)
• Infrared Temperature Measurement: Theory and Application
• Principles of Infrared Thermocouples (PDF file)
• Table of Total Infrared Emissivity (PDF file)
• Frequently Asked Temperature Questions (PDF file)
• Introduction to Temperature Measurement
• Temperature Measurement and Control Glossary
• Practical Guidelines for Temperature Measurement
• Temperature Conversion Chart Between C and F
See all Technical Reference

When selecting noncontact temperature measurement instruments, it is necessary to take into account not only the target and its emissivity, but also the surroundings and the invtervening atmosphere.

Sign up for the omega.com e-mail newsletter!
Click here for help finding your product!
The Infrared Thermometer
How does an infrared thermometer work?
The most basic design consists of a lens to focus the infrared (IR) energy on to a detector, which converts the energy to an electrical signal that can be displayed in units of temperature after being compensated for ambient temperature variation. This configuration facilitates temperature measurement from a distance without contact with the object to be measured. As such, the infrared thermometer is useful for measuring temperature under circumstances where thermocouples or other probe type sensors cannot be used or do not produce accurate data for a variety of reasons. Some typical circumstances are where the object to be measured is moving; where the object is surrounded by an EM field, as in induction heating; where the object is contained in a vacuum or other controlled atmosphere; or in applications where a fast response is required.

Using an Infrared Thermometer FAQ's:

Why measure temperature with an infrared thermometer?
Infrared pyrometers allow users to measure temperature in applications where conventional sensors cannot be employed. Specifically, in cases dealing with moving objects ( i.e., rollers, moving machinery, or a conveyor belt), or where non-contact measurements are required because of contamination or hazardous reasons (such as high voltage), where distances are too great, or where the temperatures to be measured are too high for thermocouples or other contact sensors.

What to consider when selecting an infrared thermometer?
The critical considerations for any infrared thermometer includes field of view (target size and distance), type of surface being measured (emissivity considerations), spectral response (for atmospheric effects or transmission through surfaces), temperature range and mounting (handheld portable or fixed mount). Other considerations include response time, environment, mounting limitations, viewing port or window applications, and desired signal processing.

What is meant by Field of View, and why is it important?
The field of view is the angle of vision at which the instrument operates, and is determined by the optics of the unit. To obtain an accurate temperature reading, the target being measured should completely fill the field of view of the instrument. Since the infrared device determines the average temperature of all surfaces within the field of view, if the background temperature is different from the object temperature, a measurement error can occur. OMEGA offers a unique solution to this problem. Many OMEGA infrared pyrometers feature patented laser switchable from circle to dot. In the circle mode a built-in laser sighting creates a 12-point circle which clearly indicates the target area being measured. In the dot mode a single laser dot marks the center of the measurement area.

OMEGA Infrared Pyrometer with Built-In Dot/Circle Switchable Laser Sighting


Emissivity, and how is it related to infrared temperature measurement.
Emissivity is defined as the ratio of the energy radiated by an object at a given temperature to the energy emitted by a perfect radiator, or blackbody, at the same temperature. The emissivity of a blackbody is 1.0. All values of emissivity fall between 0.0 and 1.0. Most infrared thermometers have the ability to compensate for different emissivity values, for different materials. In general, the higher the emissivity of an object, the easier it is to obtain an accurate temperature measurement using infrared. Objects with very low emissivities (below 0.2) can be difficult applications. Some polished, shiny metallic surfaces, such as aluminum, are so reflective in the infrared that accurate temperature measurements are not always possible.

Five Ways to Determine Emissivity
There are five ways to determine the emissivity of the material, to ensure accurate temperature measurements:
  1. Heat a sample of the material to a known temperature, using a precise sensor, and measure the temperature using the IR instrument. Then adjust the emissivity value to force the indicator to display the correct temperature.
  2. For relatively low temperatures (up to 500°F), a piece of masking tape, with an emissivity of 0.95, can be measured. Then adjust the emissivity value to force the indicator to display the correct temperature of the material.
  3. For high temperature measurements, a hole (depth of which is at least 6 times the diameter) can be drilled into the object. This hole acts as a blackbody with emissivity of 1.0. Measure the temperature in the hole, then adjust the emissivity to force the indicator to display the correct temperature of the material.
  4. If the material, or a portion of it, can be coated, a dull black paint will have an emissivity of approx. 1.0. Measure the temperature of the paint, then adjust the emissivity to force the indicator to display the correct temperature.
  5. Standardized emissivity values for most materials are available (see pages 114-115). These can be entered into the instrument to estimate the material’s emissivity value.
How can I mount the infrared pyrometer?
The pyrometer can be of two types, either fixed-mount or portable. Fixed mount units are generally installed in one location to continuously monitor a given process. They usually operate on line power, and are aimed at a single point. The output from this type of instrument can be a local or remote display, along with an analog output that can be used for another display or control loop. Battery powered, portable infrared ‘‘guns’’ are also available; these units have all the features of the fixed mount devices, usually without the analog output for control purposes. Generally these units are utilized in maintenance, diagnostics, quality control, and spot measurements of critical processes.
 Infrared Thermometer Types
OS530L Handheld Infrared Thermometer Handheld Infrared Thermometers
Handheld infrared thermometers are one of the most popular types of infrared pyrometer. They are commonly used for portable applications although some models also feature an integral tripod mount. OMEGA offers a large variety of infrared thermometers in various shapes and form factors. Many of OMEGA handheld infrared pyrometers feature OMEGA's patented Circle Dot/Circle Laser sighting which clearly outlines the field of view of the thermometer.

OS643 Pocket/Stick-Type Infrared Thermometer Pocket/Stick-Type Infrared Thermometers
Pocket or stick type infrared thermometers are extremely compact. They are normally small enough to be carried in a shirt pocket.
OS36 Infrared Thermocouples Infrared Thermocouples
Infrared thermocouples are small low cost infrared sensors. They are unique in that they are self-powered and produce an output that mimics a thermocouple sensor.
Fixed Mount Infrared Thermometers/Fixed Mount Infrared Transmitters Fixed Mount Infrared Thermometer/Transmitters
Fixed mount infrared thermometers are commonly used in industrial processes where the thermometer can be mounted in a stationary position. Read the High Speed Fiber Optic Infrared Transmitter article for information about the OS4000 Series.
IR2 Two Color-Ratio Thermometry Two Color-Ratio Thermometry
Given that emissivity plays such a vital role in obtaining accurate temperature data from infrared thermometers, it is not surprising that attempts have been made to design sensors which would measure independently of this variable. The best known and most commonly applied of these designs is the Two Color-Ratio Thermometer. This technique is not dissimilar to the infrared thermometers described so far, but measures the ratio of infrared energy emitted from the material at two wavelengths, rather than the absolute energy at one wavelength or wave band. The use of the word "color" in this context is somewhat outdated, but nevertheless has not been superseded. It originates in the old practice of relating visible color to temperature, hence "color temperature."
^top  
Automation | Accelerometers | Calibrators | Cartridge Heaters | Chart Recorders | Cryogenics | Custom Pressure Transducers | Data Loggers | Data Acquisition | Dial Thermometers | Fiber Optics | Flexible Heaters | Flowmeters | Glass Bulb Thermometers | Grippers | Heaters | Humidity Measurement | Immersion Heaters | Infrared Thermometers | Level Measurement | Load Cells | Magnetic Flow Meters | Panel Meters | Pressure Gauges | Pressure Transducers | Rotameters | RTD| Signal Conditioners | Stepper Motors | Strain Gages | Strip Heaters | Temperature Controllers | Temperature Labels | Temperature Measurement | Temperature Sensor Manufacturing | Temperature Transmitters | Thermistors | Thermocouple | Thermocouple Wire | Thermowell | Ultrasonic Flow Meters
Home Page Order by part number Free Literature Search About OMEGA Engineering