Back to omega.ca
Temperature Measurement
 
   Temperature Measurement - an Introduction



Product Links
View All Temperature Measurement Products
Thermocouple Probes and Assemblies
RTD Probes, Elements and Assemblies
Thermistor Elements, Probes and Assemblies
Fixed Mount Infrared Thermometer/
Transmitters
Glass Bulb and DialTempTM Thermometers
Indicating Labels, Crayons, Cements and Lacquers
Infrared Temperature Measurement Instruments
Technical Links
Technical Library for Temperature Measurement
Infrared Temperature Measurement
Technical Library for Temperature Measurement

Temperature Measurement:

How does one measure temperature? Temperature measurement can be accomplished using a variety of sensors and devices. All of them ascertain temperature by sensing some change in a physical characteristic. The following methods an engineer is likely to come into contact are: thermocouples, resistive temperature devices (RTDs and thermistors), infrared radiators, bimetallic devices, liquid expansion devices, and change-of-state devices.


SA1XL Series 5-Pack
Surface Mount Fast-Response Thermocouples: SA1XL Series 5-Pack
Achieve response times of less than 0.15 seconds! These surface thermocouples are constructed using a Kapton/ fiberglass junction insulation along with a fiberglass-insulated lead wire.
More details »


   Types of Temperature Measurement Sensors
Thermocouple Temperature Measurement
Thermocouples consist essentially of two strips or wires made of different metals and joined at one end. Changes in the temperature at that juncture induce a change in electromotive force (emf) between the other ends. As temperature goes up, this output emf of the thermocouple rises, though not necessarily linearly.

Bare SH Thermocouple Temperature Measurement Sensor
RTD - Resistance Temperature Devices
Resistive temperature devices capitalize on the fact that the electrical resistance of a material changes as its temperature changes. Two key types are the metallic devices (commonly referred to as RTDs), and thermistors. As their name indicates, RTDs rely on resistance change in a metal, with the resistance rising more or less linearly with temperature. Thermistors are based on resistance change in a ceramic semiconductor; the resistance drops nonlinearly with temperature rise.
F Series Resistance Temperature Device (RTD) Elements Thin Film Platinum
Infrared Temperature Measurement Devices (IR)
Infrared sensors are noncontacting devices. They infer temperature by measuring the thermal radiation emitted by a material.
OS532 Infrared Temperature Measurement Device
Bimetallic Sensors and Devices
Bimetallic devices take advantage of the difference in rate of thermal expansion between different metals. Strips of two metals are bonded together. When heated, one side will expand more than the other, and the resulting bending is translated into a temperature reading by mechanical linkage to a pointer. These devices are portable and they do not require a power supply, but they are usually not as accurate as thermocouples or RTDs and they do not readily lend themselves to temperature recording.
AR DIALTEMP BiMetallic Temperature Measurement Device
Fluid-Expansion Thermometers
Fluid-expansion devices, typified by the household thermometer, generally come in two main classifications: the mercury type and the organic-liquid type. Versions employing gas instead of liquid are also available. Mercury is considered an environmental hazard, so there are regulations governing the shipment of devices that contain it. Fluid-expansion sensors do not require electric power, do not pose explosion hazards, and are stable even after repeated cycling. On the other hand, they do not generate data that is easily recorded or transmitted, and they cannot make spot or point measurements.
GT 736000 Sereis Glass-Bulb Thermometers
Change-of-State Temperature Devices
Change-of-state temperature sensors consist of labels, pellets, crayons, lacquers or liquid crystals whose appearance changes once a certain temperature is reached. They are used, for instance, with steam traps - when a trap exceeds a certain temperature, a white dot on a sensor label attached to the trap will turn black. Response time typically takes minutes, so these devices often do not respond to transient temperature changes. And accuracy is lower than with other types of sensors. Furthermore, the change in state is irreversible, except in the case of liquid-crystal displays. Even so, change-of-state sensors can be handy when one needs confirmation that the temperature of a piece of equipment or a material has not exceeded a certain level, for instance for technical or legal reasons during product shipment.
TL-10 Change-of-state Temperature Measurement device
Automation | Accelerometers | Calibrators | Cartridge Heaters | Chart Recorders | Cryogenics | Custom Pressure Transducers | Data Loggers | Data Acquisition | Dial Thermometers | Fiber Optics | Flexible Heaters | Flowmeters | Glass Bulb Thermometers | Grippers | Heaters | Humidity Measurement | Immersion Heaters | Infrared Thermometers | Level Measurement | Load Cells | Magnetic Flow Meters | Panel Meters | Pressure Gauges | Pressure Transducers | Rotameters | RTD| Signal Conditioners | Stepper Motors | Strain Gages | Strip Heaters | Temperature Controllers | Temperature Labels | Temperature Measurement | Temperature Sensor Manufacturing | Temperature Transmitters | Thermistors | Thermocouple | Thermocouple Wire | Thermowell | Ultrasonic Flow Meters