Ideal for batch processes where a set process time is known. The charts are normally designed to rotate in standard time periods, such as 1 hour, 24 hours, 7 days, etc., although many recorders are flexible enough to accommodate non-standard time periods.
Similar to Vertical Recorders, flatbed recorders are ideal for use in research, development and production, as well as in service and education applications.
Well suited for recording of continuous processes, sections of the paper can be torn off and archived for future reference. Strip chart recorders are commonly used in laboratory as well as process measurement applications.
XY recorders accept two inputs and create a chart or graph of one input versus the other. They are commonly used to determine the relationship between the two inputs.